以前用过TL494,但是494不带PWM调光功能,因此PASS
我们公司代理各种液晶屏,所以要求驱动的芯片尽可能的通用
要求,输入电压7-18V(一般为12V)
输出电压9-60V
输出电流可达到1A
要求可以PWM调光,要SOP封装,容易采购到,温度-40到125
我也主要是 该怎么搜
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
根据你的需求,你需要一个BUCK-Boost结构的LED Driver,但是这样的IC不好找,建议固定输入电压(如通过BUCK将输入定为6V),然后用Boost mode 的LED Driver实现,可以看看TPS92692
关于搜索,你可以直接在官网上输入LED Driver搜索