This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610 Power Selector相关问题,急!



设计与Datasheet Page2中提供的参考类似,3串锂电池,正常充电和DC IN供电问题不大。但发现一种情况是不大正常:电池充电设定电压为(1+500/100)*2.1=12.6V,当电池不存在时,而Adapter(实际可能是10V~28V直流电源输入,允许电压低于电池电压工作,即使电池充不满)供电DC_IN低于12.8V时,输出到系统的电压开始跳变不稳定,后续系统不能正常供电工作,ACFET没有稳定的打开。同时挂在/PG脚上的指示灯有闪烁,并伴有能听到较明显的噪声。

当调低电池充电反馈电压力由12.6V->10.7V时,DC_IN在11V以上都是可以稳定输出,正常工作。查看DATASHEET好像没有明确的说过这一块问题,我们的设备要求可使用12V在ADAPTOR端供电让系统工作,可无电池存在,有电池存在时这种情况下也无必须充电完成要求。

请问以上现象是否属于正常现像,是否有什么方法可以解决,解决电池不存在,DC_IN可在9~12.8V稳定供给系统电源工作(即让ACFET完全导通,不作切换)