请问怎么用LM2588-ADJ做成输入5-12V(或者合适的电压)输出-24V/1A?
或者用图1flybuck的方式直接产生正负24V,希望的电流在500ma左右。
我没有找到标准的输出正负24V的变压器,我的想法是,如果用flybuck的话,我输入12V,那我就选一个1:2的变压器,按照图1的方式连接变压器,在feedback脚用电阻分压得到+24V,在变压器副边另一端得到-24V,可是不知道这个电流怎么样才能达到我要求500ma左右甚至更大一些
图1:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
谢谢您的回复。
1、如果我用12V输出,LM2588-ADJ的输出能达到500ma,甚至1A吗?我怎么样才能知道一个具体的数据
2、我都打算自己设计反激变压器,在看TI邵博士的反激变压器资料。
3、请问您是怎么用webench选择指定的LM2588芯片进行设计的?我每次用webench就是因为每次给的电路不是我想用的芯片,我就觉得他不好用
您可以告诉我是怎么选择LM2588进行设计的吗?我按照输入12V输出正负24V条件,给我推荐的电路里都没有LM2588