This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54531电容使用

Other Parts Discussed in Thread: TPS54531

TPS54531 使用WEBENCH进行设计推荐电路中输入端使用4.7UF的电容,现在我这边后端输出是负载端是变化的,而输入端电源在起始供电时会出现瞬间压降,请问输入端需要加大电容吗100UF的,之前加了三个但不清晰有和无的作用是否明显,因此请问输入端输出端带载电容如何设计更好,谢谢

  • Hi

        可以再原有的基础上将输入输出电容都加大一些。

       输入可以再增加一个10uF或者22uF,  输入电容都需要尽量靠近芯片Vin脚。 如果此时输入电压还在下拉,那么你需要确认前一级电源的输出能力,输入走线宽一点。

       考虑到你输出电流的波动,如果波动较大,可以适当加大输出电容,例如多并联一个47uF电容,不过此时你补偿也要修正。 为加快动态响应,可以再高边电阻上并联一个小电容。

  • 前一级电源下拉是瞬间的,只是在启动时因为要打火,因此会出现瞬间压降,为了保证瞬间压降不会对TPS输出造成影响因此输入电容需要加大吗,之前是使用了两个100UF的电容,请问有必要这么大吗,还有输出端为后端供电,TPS的带载能力是够的,需要加2个100UF的电容吗,谢谢您,100uf的电容是不是有点多余而且降低响应速度。

  • Hi

       这个是需要测试效果,通过测试确认,主要是由你前一级电源决定,对于TPS54531而言,前一级电压是稳定的,10uF就足够。

       不稳要看不稳定的程度,只要测试才可以确认到。