This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895充电问题 急求!!!

Other Parts Discussed in Thread: BQ25895


1、输入源为+5V和GND,D+和D-悬空未接,测出SYS管脚电压为3.67V,REGN管脚电压为5.05V,BAT管脚电压为3.85V,这些管脚电压均正常,可测出ILIM管脚电压为2.06V,此时ILIM管脚对地接了一个130Ω的电阻,按照资料上所说,当ILIM管脚电压为0.8V时,输入电流的最大值等于390/130;当ILIM管脚电压小于0.8V时,输入电流的最大值为(390×VILIM)/(RILIM×0.8V)。请问此时ILIM管脚电压为2.06V,即大于0.8V,那么此时最大输入电流限制为多少???将ILIM这个管脚的对地电阻改为67KΩ,测量该管脚电压为0.63V,这样调整是否正确,这样的阻值调整与资料推荐的不相符,为什么???
2、请问BQ25895与单片机进行I2C通讯前,需要哪些其他条件吗??我们单片机用SYS管脚供电,SDA与SCL均用10K电阻上拉到SYS管脚,给BQ25895充电芯片用5V和GND两根线供电,结果通讯一直无法接通,即单片机先写BQ25895的从机地址0x6a,但一直无法收到应答信号。。请问是什么原因??
3、I2C时序正确,用单片机测过能与其他芯片通讯,但无法与BQ25895通讯。。。。。。。

  • 1. BQ25895 可以通过WEBENCH 进行设计,请按照想要的指标得到参考的设计图看是否和目前使用的电路图有差异,同时检查一下焊接和layout是否有异常,http://www.ti.com/product/BQ25895?keyMatch=BQ25895&tisearch=Search-EN-Everything

    2.不需要其他的特殊条件,可以先使用断开VBUS输入,只接电池上去,看一下I2C是否输入正常,如果还有问题示波器抓取一下I2C波形