This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895充电问题 急求!!!

Other Parts Discussed in Thread: BQ25895

1、输入源为+5V和GND,D+和D-悬空未接,测出SYS管脚电压为3.67V,REGN管脚电压为5.05V,BAT管脚电压为3.85V,这些管脚电压均正常,可测出ILIM管脚电压为2.06V,此时ILIM管脚对地接了一个130Ω的电阻,按照资料上所说,当ILIM管脚电压为0.8V时,输入电流的最大值等于390/130;当ILIM管脚电压小于0.8V时,输入电流的最大值为(390×VILIM)/(RILIM×0.8V)。请问此时ILIM管脚电压为2.06V,即大于0.8V,那么此时最大输入电流限制为多少???将ILIM这个管脚的对地电阻改为67KΩ,测量该管脚电压为0.63V,这样调整是否正确,这样的阻值调整与资料推荐的不相符,为什么???
2、请问BQ25895与单片机进行I2C通讯前,需要哪些其他条件吗??我们单片机用SYS管脚供电,SDA与SCL均用10K电阻上拉到SYS管脚,给BQ25895充电芯片用5V和GND两根线供电,结果通讯一直无法接通,即单片机先写BQ25895的从机地址0x6a,但一直无法收到应答信号。。请问是什么原因??
3、I2C时序正确,用单片机测过能与其他芯片通讯,但无法与BQ25895通讯。。。。。。。

  • 1、BOOST模块不需要,所以PMID和OTG管脚悬空,请问这种情况是否会引起充电问题???

    2、SYS管脚为单片机供电,通讯已正常。但是将充电使能之后,即CHG_CON置1后,电池无法充电,输入电压为5V,输入电流一直为20mA,输入电流过低,请问什么原因???

  • 1. PMID管脚上的电容不能省略,OTG对充电影响不大,不过建议还是给一个固定的电平

    2. 这种调试建议打印出charger的寄存器,查看是不是出现了fault,重点看一下REG0B和REG0C。