This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD3138A64快速中断怎么设置?我想设置快速中断fault3,可是利用下面的代码没有实现,还请大神能够指点下,问题出现在哪



 TimerRegs.T16PWM2CMP0DAT.all =1562;   //40hz 1562;   //Threshold to reset counter - 15.625 mHz/10 KHz.
 TimerRegs.T16PWM2CMPCTRL.all = 2;  //Enables compare 0 (reset) interrupt
 TimerRegs.T16PWM2CNTCTRL.all = 0x00c; //PWM counter is running & enables PWM counter reset by compare action on compare 0
 disable_fast_interrupt(); //make sure fast interrupt is disabled
 disable_interrupt();
// write_reqmask(CIMINT_ALL_PWM2_COMP);    // | CIMINT_ALL_FAULT_PIN);
 write_reqmask(CIMINT_ALL_FAULT_PIN|CIMINT_ALL_PWM2_COMP);//(0x02020000); //enable FAULT_INT and PWM0_INT
 write_firqpr (CIMINT_ALL_FAULT_PIN);                     //(0x02000000); //make them all irqs except FAULT_INT
 enable_fast_interrupt(); //make sure fast interrupt is enabled for OVP shutdown
 enable_interrupt();