如何把LM337电压输出调整为0V,是否可以在ADJ端加+1.2V电压?是否可以抵消掉本身的基准电压?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Vout与Vadj之间保持1.2V压差,而不是像其他电源芯片那样Adj是一个1.2V的基准参考,所以是不可以直接Adj加1.2V来做控制的。
正常芯片工作的时候,当ADJ电压为0V,VOUT输出为-1.2V,VOUT与ADJ端电压压差为-1.2V, 我想在ADJ端加电压为1.2V,VOUT要与ADJ电压保证-1.2V的压差的话,输出应该是0V才对,不知道这样理解是否可以?