This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大神们提供一个12V转±5V的方案吧,正的有200ma,负的50-100ma就行
Hi
用TPS54140, 参考设计方案: http://www.ti.com.cn/cn/lit/an/slva369a/slva369a.pdf (TPS54140是42V输入版本,你只需要17V以上,所以可以不用60V的TPS54160)
我想要的是12V转的。。我看这个芯片是18V-30V的输入啊
这个是设计案例, 12V也是满足这个芯片输入要求的,具体看一下datasheet.