This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28740 這個IC pin8接大於 DC700V 該如何處理

Other Parts Discussed in Thread: UCC28740

UCC28740 這個IC pin8接> DC700V 該如何處理Buck Voltage Max 700V, 但目前我的Buck Voltage是760V~800V左右,該如何處理,直接接到Buck Voltage上,謝謝。

  • Hi

       之所以是700V,是因为芯片这个脚只能承受700V的高压,所以要么就是将其降下来,要么就找更高电压的方案。

       这个电路或者对你有启发:http://www.ti.com.cn/cn/lit/an/zhct112/zhct112.pdf (输入电压是可以加高,对应的MOS之类的器件也需要选择更高电压的管子)