Other Parts Discussed in Thread: TPS61042, TPS61160, TPS62160, TPS61166
输入电源5V左右;
应用环境为工业现场;
要求能PWM调光;
工作的典型状态是:180mA,9.6V
输出电压范围是8~11V
对封装没什么要求,外围器件越少越好
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以看看TPS61042,Vin=1.8 V to 6 V, Boost Mode,Imax=500mA,外围器件非常少
Hi
TPS62160: http://www.ti.com.cn/cn/lit/ds/symlink/tps61160.pdf
TPS61166: http://www.ti.com.cn/cn/lit/ds/symlink/tps61166.pdf