This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

当BQ25890H电池的电压低于3.55V时,ADC无法读取BAT和SYS的电压?



请教TI技术支持,我们现在使用BQ25890H遇到一个问题:

问题:当电池电压大概低于3.55V以下,使用BQ25890H内部ADC无法读取BAT和SYS的电压,读取0x0E和0x0F总是零。

           寄存器0x02已经设置为0x5D。寄存器0x07已经设置为0x8D,关闭watchdog timer。

如果电池高一点,大概3.6V左右,又可以正常读取ADC值,或者插入充电器,也可以支持读取ADC值。

请问,这可能是什么原因导致的?