hello!
如题,输出电流不大,常规500mA或是1A就可以,有没有合适的型号推荐呢?谢谢~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
如果用一个芯片的话,可以考虑用TPS54560+ 耦合电感的方式,参照这个设计: http://www.ti.com.cn/cn/lit/an/slva369a/slva369a.pdf
或者回扫式稳压器 LM2587之类: http://www.ti.com.cn/cn/lit/ds/symlink/lm2587.pdf 也是通过变压器得到2个电压。
如果用2个芯片做,正电压可以用降压芯片,选择很多,例如TPS62150A之类
负电压也可以选择降压芯片来做,但是要选择大于17V输入的芯片,你可以选择TPS54335/6这样的降压芯片,或者TPS5420 : http://www.ti.com.cn/cn/lit/an/slva257a/slva257a.pdf
TPS54560,这个是18-36V输入的,12V用不了啊?
你好,
可以考虑buck转buck-boost实现12V转正负5V,比如利用两颗LMR16030来实现即可。具体实现电路可以参考附件
Hi
对于供电的电压要求比较高的应用,都是建议在DC/DC后再增加一级超低Noise高PSRR的LDO的。
下面是LM27761的测试结果,可以看到,输出电流越大,输出电压越低,这是正常现象,你是给运放供电,如果运放用于信号采集的话,负载电流很小,输出电压的跌落也会比较小,只要运放的输出电压在供电电压范围内就没什么问题。
Vin(V) | Vout(V) | Iout(A) |
5.08 | -4.95 | 0 |
5.08 | -4.97 | 0.05 |
5.07 | -4.87 | 0.1 |
5.07 | -4.77 | 0.15 |
5.07 | -4.66 | 0.2 |
5.07 | -4.56 | 0.25 |