Other Parts Discussed in Thread: TPS652510
TPS652150中3个VIN必须同时接电源或者接相同电源,不能VIN1先接通产生VOUT1后,VOUT1再作为VIN2和VIN3吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS652510
TPS652150中3个VIN必须同时接电源或者接相同电源,不能VIN1先接通产生VOUT1后,VOUT1再作为VIN2和VIN3吗?
从功能框图来看,其内部的时序逻辑是由Vin2来供电,所以无法单独使用Vin1和Vin3,必须先使用Vin2,才能使用Vin1和Vin3。具体的建议你通过实验确认
不好意思 我写错了 是TPS652510 使用手册里没有提示必须VIN2先上电 看框图好像是要其先上电 对吗?
框图显示是这样,具体是怎样我正在咨询,有了结果会回复你的
Hi
我觉得Vin可以用独立电源,也就是说可以将其中一路输出给到另外一路输入。(三路是独立的)
但是Vin2必须要先给,原因是这个供电时要产生7V/3V 两个偏执电压,这个是给到芯片内部供电的,其他2组是会用到的。如果后给Vin2, Vin1/Vin3或无法启动。
你好, 这边帮你问了,你说的这种用法我们没有试过,需要你自己去实验验证,根据原理图,应该是可以的,只要VIN2先上电就可以。
你具体的应用场景是什么呢? 为什么要这么用呢?谢谢