您好,请教个问题
1.在按照下图之电路布线后,输入改为稳定3V的直流电压,发现
电阻分压的这几个输出脚位PIN7、8、10、11、12之输出电压都为0.45V~0.50V之间,
等于此些接脚为短路,不知问题为何。
2.另外个问题是VOUT输出端之电压一直低于1V无法提供更高电压做输出。 以上问题请教,感谢。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.