见附图,为bq769x0(bq76920、bq76930、bq76940)
请教:
bq769x0 REGOUT的带负载能力 是多少mA ?
谢谢 !
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你可以参考datasheet里的EXTERNAL REGULATOR部分。从发热角度考虑,建议控制在10mA以内
Hi
38mA的条件是 REGOUT = 0 V,这个相当于是短路电流。
按照参数表上的条件,最大有20mA, 在这个范围内用时保险的。
谢谢 !
在datasheet中,没有找到20mA 这个数值呀