hi,你好,TI,我想请教一下,如果要实现23V-29V的输入,输出固定在24V 10A或以上的情况,是否使用LM5022这个芯片可以?这里涉及到一个低于24V的和高于24V的问题。输入来源于大容量电池。请不吝赐教,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,如果你是小电流可以采用全集成的芯片,但是你的输出功率很大,有240W以上,所以还是需要采用LM5175的BUCK_BOOST工作方式,你可以利用WEBENCH软件进行辅助设计,内部提供原理图以及PCB,非常方便。建议你采用LM5176,是5175的升级版,稳定性会更出色。