各位TI的达人:
我最近想选用TPS65261( 3A/2A/2A Output Current)作为系统的电源,我的系统需要1路1V的电压,电流最大为2.8A,我想用TPS65261输出3A的那个通道输出1V,2.8A,另外2路电流不大,几百MA到1A, 不知道实际使用会不会有什么问题,感觉3A这个通道裕量不多?这种多通道设计应该注意哪些方面?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位TI的达人:
我最近想选用TPS65261( 3A/2A/2A Output Current)作为系统的电源,我的系统需要1路1V的电压,电流最大为2.8A,我想用TPS65261输出3A的那个通道输出1V,2.8A,另外2路电流不大,几百MA到1A, 不知道实际使用会不会有什么问题,感觉3A这个通道裕量不多?这种多通道设计应该注意哪些方面?
Hi
没有问题,主要负载不要超过3A.
电路layout都可以参考EVM板: http://www.ti.com.cn/cn/lit/ug/slvua03/slvua03.pdf
没问题,需要注意的就是电路的补偿元件选择,不过这个可以利用WEBENCH进行参考设计。布局布线按照User Guider来设计