This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教UC2902负载均流方案问题

Other Parts Discussed in Thread: UC2902, TPS54360

uc2902的官方推荐接法是对DCDC模块进行均流;但我现在的输入电压范围比较宽,12~48V输入,市场上该类DCDC模块较少;同样要求隔离的输入;所以采用先降压,然后再用变压器隔离的方式;降压芯片采用TPS54360,输出11V电压,然后作为推完形变压器的输入,变压器输出15V;我在变压器的输出端用uc2902进行负载均流,调整放大器的输出经过线性光耦反馈到TPS54360的FB端,不知道这种方案是否可行。

   

  • HI  

        你做多大功率,需要先降压,在隔离,还并联均流?

  • 您好,请教一个问题:请问在一个电源板中,有多个电压输出,3.3V,5V,12V,它们共用一个GND,每路电压都接了UC2902均流芯片,请问每路电压的电流在流经检测电阻时走的回路会被其他电压的回路影响吗?每路电压的均流精度会有影响吗?

    希望能得到您的回复,谢谢。

  • 不可以,你需要调整的是推挽电路的占空比,而不是降压电路的占空比,除非你的后级推挽是固定占空比的。

x 出现错误。请重试或与管理员联系。