This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

主动均衡EMB1428和EMB1499 相关问题



请问

1)在EMB1428手册中Table 3/P22 中fault[3:0]=1010时,FAULT_INT triggered为什么是YES?

2)用EM1402的评估板,自己焊接EMB1428和EMB1499主动均衡部分,CPU发出去的是0x10,EMB1428返回的为0xA1,感觉通信部分应该没错,但是CELL switch对应的MOS管并没有打开,量参考设计C46两端的电压为0.

说明CELL SWITCH 和POLARITY SWITCH均没有动作,否则C46两端的电压应该为电池组中一节电池的电压。

3.故障fault[3:0]=1010是否为有错误,如果有错误改怎么解决?fault[3:0]=1110这个错误改怎么解决?手册中给出了故障码,并没有给出故障的解除办法。

4.EMB1428中VDDIO的供电电压为5V可以吗?SPI通信的速率恒定为1MHZ吗?

5.想知道EN,DONE,DIR,DIR_RT这几个管脚在能够充放电时的时序图。

谢谢!