This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61021A升压模块的输出电压问题

Other Parts Discussed in Thread: TPS61021A


请问,按照TPS61021A模块的典型电路设

计,原理图如下,为什么在输入是1.8~3.2V的时候,输出不是3.3V,而是3.5V呢?请大侠指教

  • Hi

        用示波器看一下,3.3V是否是不稳定的,所以导致万用表测量导致示数偏高?

        在你的电路中不需要用电感隔离功率GND和模拟GND, 建议换成0欧姆,或者用短导线连接,看能否正常?

        如仍不能稳定,再确认你的layout,  可参照datasheet.

  • 请问输入1.8~3.2V,输出3.3V的TPS61021A典型电路可带动最大多少安培的负载?若负载正常工作最大160mA,TPS61021A能否带动正常工作,输出3.3V?

  • Hi  

        最大负载能力与输入电压曲线图如下:

        

       红线是3.3V输出,从曲线上看最大输出电流在1.5A以上。

     (但是这个曲线可能不是按照最小3A的电流限制的结果算出来的,实际建议带载不要超过1.2A。 如果你只是要带200mA以内负载,绝对没有问题。 Layout上注意你需要注意必须有足够的输入电容尽量靠近电感输入端,其次电感的饱和电流需要足够大)