This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DRV8432 RDS问题



根据官方PDF文档第一页显示Rds为110mΩ,如下图所示:

但是在文档第9页的图表中正常的Rds为1欧,前后矛盾啊,到底以哪个为准呢?

  • Hi 

        110mohm是对的。

         底下图纵坐标的单位不是欧姆,而以一个比值, 是Rdson/Rdson(12V)的比值。  所以横坐标是12V时刚好是1,而8V时比值是1.083左右,代表此时的Rdson是1.083* Rdson(12V)。