This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610在电池未接的情况下,STAT1灯长亮什么原因啊?

Other Parts Discussed in Thread: BQ24610

BQ24610在电池未接的情况下,STAT1充电中)灯长亮什么原因啊?

经过测试,输入ACDRV保持低电平,导通输入级的PMOS管,

然后HIDRV的对应MOS管保持低电位,推挽电路终止,输出电压1.6v,

BATDRV保持高电位,截止

REGN为5.9V,BTST为7.3V

设置点,输入级ACSET为0.53V,

ISET1/2均为0.2v

谢谢~

  • 想知道哪个引脚或者功能故障才会导致这个?

    基本上能确定是PCB造成的,因为重新焊接或更换所有的MOS管跟芯片故障现象依旧,重新焊接所有贴片器件故障依旧,更换PCB后,问题消失....但是我测的每个监控点的电压没有任何问题

  • 朋友,我建议你用的是什么型号的MOS管,N沟道和P沟道都要仔细看一下参数,是不是导通电压太高了?

    你这种情况,可能是芯片的引脚电压驱动不了你的MOS管。