This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求推荐一款LED的恒流源驱动



输入12V,要求可以通过PWM调闪烁频率(最高500HZ),同时要求可以通过输入一个模拟电压(0-5V或者0到3.3V)去控制LED(8x12个灯,每个灯都是并联的,灯的压降在3.3V左右)阵列的亮度。PWM占空比百分之99,灯的亮度调到最大时,电流是1.6A。