This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3895控制能否做成全电压范围输出的电源



UC3895控制能否做成全电压范围的电源?最近要做400V三相输入,输出0-6KV,电流1A的电源。就是不知道移相控制,能否实现从0到6kV全范围可调节。若不能,有无好的拓扑或控制芯片可推荐

  • 亲;作为IC;可以达到0-100%移相,但是作为电源还会收到空间电磁场干扰而略有输出。比如;你要做到绝对0A时0V输出,那是不可完成的工作。所以;这个问题的答案;最后还要亲亲自解决。IC只能保证亲有足够的移相空间而已。

  • 不需要0V0A绝对输出,只是要做到在一定范围内,电压能连续可调。因为移相全桥有一定的占空比损失,担心其电压连续调整能力。用PWM可以做到,但因为是硬开关,效率做不高。现在做方案,所以想问同行有无做过这方面的成功案例。