This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq24075t无法充电问题

Other Parts Discussed in Thread: BQ24075T, BQ24075

Hello 大家好!

       我现在用的充电管理的芯片是bq24075t的芯片给锂电池充电。

       但是现在无法给电池进行充电,原理图如下:

       

   VBAT是接入的4.2V锂电池,IN是USB的电压,测量是5V,SYSOFF ,CHG,PGOOD是接入到主MCU上的。

  问题:

   1.请TI的大神能不能看看原理图有不合理的地方?因为现在无法充电,谢谢。

   2.我看了datasheet,TS是需要接入NTC电阻的,这个是必须的吗?板子上现在接入的是一个10K的普通电阻。

   3.充电的时候检测到ISET接入的电阻上的电压是0 , 证明是没有充电电流吗?

   4.充电的时候SYSOFF主控是已经拉低的,并且插入USB上后CHG也是有信号检测到的,PGOOD上信号也是正常的,但是就是不能正常的充电。

   5.另外还有想问下TI的大神,这个芯片怎么进入低功耗模式?需要配置哪些引脚?我现在测试功耗还是比较大的,几十个uA,但是我看datasheet有一个睡眠模式是6uA,请问如何配置管脚可以进入这个睡眠模式。