Other Parts Discussed in Thread: BQ24610, TPS40210
用BQ24610按照参考设计做了一款3节锂电池(充电电压12.6V)的充电电路,当input>13V,插入电池,整个系统可以正常工作,状态指示也是正常的;但是由于在车载应用时有可能不插入电池,且input由铅酸电池供电,有可能低于12V,这个情况下BQ24610的system端的电压只有不到11V且不太稳定,发现ACDRV会有个25HZ的梯形脉冲,BATDRV上面也有类似的脉冲。按datasheet来讲,一旦VCC电压正常后(12V左右,此时没有插入电池),ACDRV就可以正常打开P-MOS,system直接由input供电。但是我的电路却不是如此。
就高人指点一二,谢谢!