This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
为何我的充电电压超过14V就不能充电,它的充电电压不是4.5---16V吗?
把电压降回14V以下之后,是否可以恢复正常充电?另外,检查一下MOSFET的耐压值是多少?
Hi
确认一下是否有造成OVP(用示波器测试一下OVPSET的电压,看是否因为noise导致过压误动作)
电压降回14V以下之后可以充的,MOS管耐压是30V的
输入电压是多少?BQ24133是降压型充电芯片,输入电压必须高于电池电压。