Other Parts Discussed in Thread: LM5030, UCC2897A
输入是DC37-57V, 输出 是20V@3A的LM5030隔离式DC-DC电源,加上同步整流后的效率大约是多少?有人用过吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
你期待的效率是多少? 或者你可以选择有源嵌位的芯片UCC2897A来做,TI有提供很多方案,有增加同步整流,效率在94%左右。
如果你是应用于POE,在你的POE芯片的“工具与软件”中找一下,看有没有UCC2897A的方案(我印象中见过)。在TI的UCC2897A的“工具与软件”的方案中没有完全符合你参数的方案,但是效率都是相对比较高的,或能达到你的要求。
这个功率等级的对于同步整流的损耗也是不能忽略的,关键看你需要多大的效率了,不会有太大的提升。