现在用mcu去和bq34z100做通信,mcu需要知道电池是空闲还是充电还是放电,去做相应不同的处理
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
8.3.1.8 AverageCurrent(): 0x0A/0x0B This read-only command pair returns a signed integer value that is the average current flowing through the sense resistor. It is updated every 1 second with units of 1 mA per bit. However, if PackConfiguration [SCALED] is set then the units have been scaled through the calibration process. The actual scale is not set in the device and SCALED is just an indicator flag.
您好,根据手册15页的描述,发送AverageCurrent()指令,通过读出来的电流的正负就可以确定是充电还是放电