Other Parts Discussed in Thread: LM2576, LM25088, TPS5430, LMZ34002, TPS54560, UC3842
求一个能输出-5V 1-2A的电源芯片,最好能和LM2576搭配使用,实现12V输入,正负5V输出。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
谢谢!麻烦再推荐个5V电源极性反向芯片,输出电流能达到0.5-1A的。我用过ICL7660,但是输出电流太小了。
Hi
buck芯片都可以做成负电压输出,这个不是坑,而是改变了芯片的转换Topy, 将Buck变化成buck-boost.
这个转换并不能说是将正电压的正接到GND, 正电压的GND就变换成负电压。
可以采用TPS5430, 如下为设计文档可以参考: http://www.ti.com.cn/cn/lit/an/slva257a/slva257a.pdf
用TPS5430的话,输入电压可以是12V吗?还有,可以同时用两片TPS5430来产生共地的一个+5V,一个-5V吗?
如果用LM2576的话,可以同时用两片TPS5430来产生共地的一个+5V,一个-5V吗?
谢谢!