使用 TPS40193DRC芯片实现12V转5V 10A,其中供电输入为12V,输出电压为0.33V不能正常工作,附上原理图,ENABLE pin这样接有问题吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
嗯是的,但是工作一小会发热非常厉害,可能是layout的问题吧?
HI
芯片底部Powerpad是需要充分与GND焊接,并且扩展GND面积用于散热。(将GND当作散热片,打孔到背面GND,Datasheet上有参考,可借鉴)
Hi
选择的MOS,Qg尽量小。( 如果温度只是70摄氏度以内都是没有问题的,毕竟芯片最高温度可以是125摄氏度,但是通常希望温度第一点,因为此时可靠度高一些)。