This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23754应用问题

Other Parts Discussed in Thread: TPS23754, TPS65251, TPS23751, TPS23754EVM-383

你好:

目前想做一款产品电源方案是TPS23754转5v,然后5V通过tps65251生成3路CPU需要使用的电压,我们的5v,MAX功耗大概有25W,如果用30w交换机供电,参考synchronous flyback topologies最大效率只有85%,如果使用这种方式,明显比较吃紧,参考datasheet上说明如果应用active clamp forward topology结构,可以提升效率,但你们的网站上没有看到针对此种应用的applicion note 和EVM报告,可否提供以下。

最后问题是:如果用active clamp forward topology结构,在5v功耗有25W的情况下,TPS23754是否合适(pse交换机输入功率30w)?