This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ27542-G1方案的基本参数写入于LOG ID问题确认?



下午好,我们的产品中使用了 BQ27542-G1电量计IC,有以下问题需要帮忙确认下(附件有设计芯片内的参数跟LOG的一个数据),谢谢!

1、首先说下基本信息,电芯初期设计容量是3200mAh,实际分容测试为3400mAh,工作模式分0.2c与0.5C两种工作模式充放电,放电截止电压为3.3V(硬件保护部分为过充4.25V,过放为2.5V),请帮忙确认下我设置的基本参数是否正确(见附件123);

2、因样品交期比较急,初步提供了几个没完成学习的电池给客户调试用,目前遇到充满电-放电-充电时电量差别很大,电压与实际电量不匹配,请问是基本参数不匹配造成的还是没学习的原因造成的?

3、基本参数的确认是以实际应用工况为准还是以电池硬件保护部分为准,另设计容量是写3200mAH还是写电芯实际3400为准;

4、化学ID怎么确认,测试流程是怎么样的?

盼复,谢谢!


20170914.rar