This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61089升压问题咨询



自己用TPS60189将4.7V~5.3V电压升到6.5V,再用REG113NA降到5V

电路原理图如下:

现在的问题是:

1、空载时5V_ACC_GYRO有5.03V左右,正常

2、加负载到5V_ACC_GYRO,负载电流约300mA时,5V_ACC_GYRO掉到了4点几V。量测6.5V_BOOST点位电压已经降到了4点几V。

请问这是什么原因呢?