稳压芯片宽输入,最高大概40-50V,输出5V,有没有用过的,可接BQ24072充电。最好周围电路小一些,板子尺寸有限。试过LMR5160与LMR16020,效果都不太好。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
你选择的这两款芯片都可以的,或者选TPS54260之类。
请问你说指的效果不好是指什么?
带负载能力差,两款稳压芯片当负载电阻降低到10欧姆时,不能稳压5V,不知道是什么原因造成的,是因为电感选型问题吗
不正常。你的电路设计有问题,原理图, BOM或者PCB有问题。
Hi
芯片的温升可以借助TI的Webench仿真获得,建议多运用一下这个工具(包括选型,获得参考电路,以及电路参数,包括效率温升等)
手触摸,发烫,负载5欧姆,输出功率5W,输入功率6.5W左右
仿真显示没问题的,选型除了电感都是根据Webench提供的选的,还有晶体管用的B380-13-F,仿真显示可用CD214B-R3600替换,但实际测了一下,发现稳压稳不住,有什么其他型号可以替换吗?尺寸要小,因为板子空间有限,谢谢