Other Parts Discussed in Thread: LM25116
现在用LM25116芯片在电流达到13A以上的时候,电感会有声音发出,这种情况需要如何调整,现在DCDC的开关频率为50KHZ,电感是10uH 25A的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM25116
现在用LM25116芯片在电流达到13A以上的时候,电感会有声音发出,这种情况需要如何调整,现在DCDC的开关频率为50KHZ,电感是10uH 25A的。
Hi
测试一下13A以上,驱动信号是否出现较大干扰(可以与5A时驱动做比较)。
可能是因为Layout, 电流做得越大,layout要求越高。
首先用WEBENCH仿真看看参数取值是否合理,看看布局是否合理(要4层板)
如果上述检查完,还是有啸叫,建议上传一下SW波形,可能是环路不稳造成