Other Parts Discussed in Thread: LMZ31520
用LMZ31520设计的12V转1V,现在输出1V正常,实测1.01V,PWRGD引脚为何一直为低?只有0.5V左右,我用的是内部上拉100K,PWRGD_PU引脚接3.3V。
之前用外部上拉100K到3.3V就没问题。知道的能解释下为什么吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LMZ31520
用LMZ31520设计的12V转1V,现在输出1V正常,实测1.01V,PWRGD引脚为何一直为低?只有0.5V左右,我用的是内部上拉100K,PWRGD_PU引脚接3.3V。
之前用外部上拉100K到3.3V就没问题。知道的能解释下为什么吗?
Hi
断电测试open drain的MOS是否击穿了?
如果没有击穿不应该有这个逻辑的。
我是不是买到假芯片了。之前用的好的片子上面字体偏小,标识48V,这次买的字体大,标识77W,能从这里判断出真假吗