Other Parts Discussed in Thread: LM5161, LM5161PWPBKEVM
目前准备做一个80V降压到5V/1A的DCDC,在评估LM5161,在看参考设计 LM5161PWPBKEVM ,对于参考设计中D1的作用不是很明白,能否去掉?哪位大神帮忙下
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM5161, LM5161PWPBKEVM
目前准备做一个80V降压到5V/1A的DCDC,在评估LM5161,在看参考设计 LM5161PWPBKEVM ,对于参考设计中D1的作用不是很明白,能否去掉?哪位大神帮忙下
Hi
评估版中D1的作用是通过输出给芯片Vcc供电,这样可以降低内部regulation的功耗。j4的目的是评估通过输出供电给电路带来的效率提升。
实际电路中,如果你的输出电压是12V左右,是建议外用输出接到VCC作为驱动供电,可以提升电路效率。
这是为了避免在VIn(如80in)和VCC(7Vcc)压差很大时LDO的损耗过大,去掉也可以,但是连着可以减小LDO上的损耗,提高效率