This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24725A设置完成之后,怎样开始充电

程序设置:

Charge Current:0x0400,对应1024mA

Charge Voltage:0x20E0,对应8416mV

Input Current:0x0400,对应1024mA

我测量了PCB的基本要求:

芯片20脚提供VIN  16V,正确。分压电阻给值也正确。
给6脚分压得到3.0v的电压,正确
6脚输出6.0V线性电压,正确
4脚输出22V,(应该正确,mos管导通了)
5脚ACOK开漏输出3.3V,正确

现在问题来了,连上电池和适配器,发现电流非常小(小于10ma),我该如何开始充电呢?是不是有配置遗漏的?