你好,
从规格书看到TPS2043B三路限流是独立的, 每路恒流是500mA?但是有个下面的描述就不知道怎么回事?
Accurate Current Limit
(0.75 A Minimum, 1.25 A Maximum)
客户实际测试单口输出时,先是系统上电,TPS2043B的EN拉低,使能好的,然后端口带负载,能带到1.5A都没有限流?不知道怎么回事?
附件原理图中EN是拉低的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
从规格书看到TPS2043B三路限流是独立的, 每路恒流是500mA?但是有个下面的描述就不知道怎么回事?
Accurate Current Limit
(0.75 A Minimum, 1.25 A Maximum)
客户实际测试单口输出时,先是系统上电,TPS2043B的EN拉低,使能好的,然后端口带负载,能带到1.5A都没有限流?不知道怎么回事?
附件原理图中EN是拉低的。
Hi Johnsin
使用的是电子负载CC档位,发现可以电流到1.5A,这样使用CC档位测试是否正确?
测试过程中输出也没短路,输出电压没有到0,只是从5V降低到4点多?