This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65185 输出电压是否稳定?

Other Parts Discussed in Thread: TPS65185

您好, 我司T65S项目在imx6sl平台开发UBOOT图片显示功能,用的是EINK的显示屏,供电芯片是TPS65185。有以下问题请帮忙确认下,
    
    问题现象: 其中有许多批次的屏是不能正常显示的,只有一小部分批次的屏以及分辨率小的屏能够正常显示。
                      针对这些显示不正常的批次的屏分析,通过万用表测量:1. 不接EINK屏的时候,是可以测量到VDDH以及VPOS的电压,分别为+25V和+15V左右。
                                                                                                      2. 接上EINK屏后,测量到VDDH以及VPOS的电压不正常几乎为0V。
                      针对这些显示正常的批次的屏分析,不管是否接EINK屏,都能测量到VDDH和VPOS的电压为+25V和+15V。
    代码做法: 在UBOOT的代码中,对TPS65185的操作,只是先把PWRUP脚拉高,然后再拉高WAKEUP脚,  然后会有一个判断PWR_GOOD电平的动作,然后就开始刷图片了。  

    想请教下,上述做法,TPS65185输出的电压是否稳定呢?有没有办法可以测量这个电压输出是否稳定。

   项目基本信息如下:
   模块 : TPS65185 
   平台:IMX6
   系统:Android 4.4.2
   显示屏: ED060KC1