您好:
請問TPS40057輸入16-35V frequency300KHz,輸出12V/5A,為什麼當我Leading到5A時,輸出電壓掉了1.5V只剩10.5V??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
KEN,
输出电压会随负载的增加而下降,如果如之前几位的讨论来看,测试方法应该是没有问题的。原因可能在于:在负载增大的同时,输入电压也会随着下降。请问使用什么电源来给TPS40057供电?有两点需要注意的是:
1. 给TPS40057供电的电源应当注意没有自身过流保护,确保提供足够多的功率给TPS40057;
2. 做测试时,因给TPS40057供电的电源的负载调整率不高,在增大TPS40057的负载时,该电源电压也会跟差下降,因此,需用用万用表时时查看该电源电压是否保持不变,如果有下降,需要调高下输入电压,在做效率测试时,也应当如此。
芯片样品申请,可以参考这个链接- http://www.ti.com.cn/general/cn/docs/gencontent.tsp?contentId=71114
评估板你可以从TI的estore购买- https://estore.ti.com/Default.aspx
同时,你也可以直接与当地授权代理商联系申请芯片和评估板,授权代理商信息如下
zong ping zhang 说:你好 请问 TPS40057 贴片 带memo board 怎样免费申请?