This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950输出问题

你好, 我做的是14.5V电压输出, 电流是50A, 这是标准的情况,但是现在是, 电流无论如何都超不多50A, 电流在49.9A时候, 输出电流源会被拉低到13.5V左右。因为随着负载的加重, 输出电流会增加, 应该是会打嗝出现, 如果在SSEN管脚加了上拉电阻,就会进入恒流模式, 现在的情况是SSEN管脚没有加上拉电阻, 只要负载加重超过50A,输出电流就会限制在50A, 电压拉低, 似乎直接进入了恒流模式,没有出现打嗝的现象 , 这是怎么回事?

2,我测试SSEN管脚电压,最大到5.4V,这点很奇怪, 是怎么产生的5.4V电压。

3,目前,似乎是有功率,却输不出来。是怎么回事呢?

谢谢