Other Parts Discussed in Thread: BQ21040, BQ25700A, BQ25703A, BQ2054, BQ2000
大家好
有没有输入5V给2节锂电池充电的芯片啊,充电电流在400mA左右的最好
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
采用2节电池并联,只有400mA, 可以选择BQ21040: http://www.ti.com.cn/product/cn/bq21040 这类相对简单的充电方案。
不好意思,对上述提问我进行更正。输入5V,对2节串联锂电池(8.4V)进行充电的芯片。
Hi
TI大部分的充电芯片BQ系列都是降压的,如果你选择升压,可以看看BQ25700A/BQ25703A.
您提到的BQ25700和BQ25703A可行;因为我正看到BQ2000和BQ2054,心存疑虑。请问,BQ2000和BQ2054能做输入5V,给2节串联锂电池供电使用吗?