This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS76801的PG引脚连接到TPS75733的EN引脚连线距离问题



我的两块板子,第一块这两个片子距离很近,使用这两个芯片实现先1.9V上电,再3.3V上电,完全可以。但是第二块板子,距离较远,PG引脚到EN引脚的连线有15cm,上电时,1.9V可以上电,3.3V无法上电,另外PG引脚无法拉低,有2.5V左右的电平。麻烦问下我第二块板子应该怎么处理。

  • David,

      在距离近的板子上时TPS76801的PG引脚接到TPS75733EN脚的电压是多少?应该高于2.2V,因为对于TPS75733有UVLO的电压为2.2V~2.75V。在距离较远的板子上,接到TPS75733EN脚的电压是多少?

    TPS78601的PG引脚是输出电压降到输出电压的92%~98%的范围内,才能拉低,请阅读数据手册的第12页。你所说的PG电压有2.5V,估计TPS78601的输出电压也差不多为2.5V,并不是1.9V。

  • 不知道你的第二块板这两个芯片的地是否共地,如果共地的话有可能是地回路太大,可以尝试用飞线将两个芯片的GND脚短接,试试效果如何。