Other Parts Discussed in Thread: BQ25895
5V的输入电压,在SYS端会有3.8v左右的输出,但是电池充电端口没有电压,REGN端口也没有电压。而且在没有输入的情况下,电池也并没有对电路供电。
我的电路板没有设计USB接口充电,D+、D-都是悬空的,会是这个影响的吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
应该不是D+D-悬空造成的,不接VBUS输入正常电池也会供电给VSYS,所以建议先检查一下电路和焊接是否有问题,包括使能管脚CE,限流ILIM等
然后通过I2C读取REG0B 和REG0C寄存器的值,看看插入VBUS时的充电状态和是否有fault