This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于半桥驱动IC LM5109B-Q1规格书中一些疑问

一、关于输入电平特性疑问

从规格书数据表格中对输入高低电平的描述看,似乎电平以1.8V为分界点区分高低电平,不像DSP或其他ic类似输入低电平最大0.8,输入高电平2.4V,高低电平直接有一定电压间隙,这样的话,5109如何在1.8V左右的输入电平中提供抗干扰能力?

二、关于驱动输出电平差值VHB-VHO

输出高电平时,在输出电流Io=0mA时,VHB-VHO值是多少:

  • Hi

       1.  1.8V是典型值,而且是25℃时的,不要关注这个,而是要看最低值0.8V,  代表要低于0.8V才是绝对的低,同样要高于2.2V才是绝对的高。

       2   Io=0mA,是指驱动输出电流吗? 其实这里和驱动电流没有关系,高边驱动输出高,VHB与VHO的压差是chargepump提供的,应该就是VDD.