This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

开关电源芯片如何选择?

Other Parts Discussed in Thread: UCC28610, TPS76201

开关电源芯片如何选择?

我要设计一个开关电源,输入电压是国际通行的100V到240V,我不知道是否可以提高到380V?

要求输出的电源是12V和5V,12V的功率是50W,5V的功率很小就可以了,不知道这种情况下我改选择什么样的芯片?是否有满足我要求的芯片呢?

  • 推荐您使用TI 的UCC28610,该芯片是一颗准谐振控制芯片,可以支持110VAC和220VAC输入,效率高,可达85%。

    在您的方案中,12V由UCC28610控制输出,5v电压可以使用稳压管搭建(如果要求低)或一颗小的LDO(比如TPS76201).