This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28700QDBVRQ1低温低输入电压不能正常启动问题

Other Parts Discussed in Thread: PMP9018, UCC28700

各位好!我使用TI的电源芯片UCC28700QDBVRQ1遇到了问题。我设计的电源规格是105VAC到260VAC,输出两路24V,稳态总功率5W(瞬态8W)。主要参考了TI的PMP9018_REVB设计。我遇到的问题是:在低温-35度的时候,电源的输入电压为105VAC,一路负载5W,另外一路空载,电源不能启动,-20度的时候可以启动。在低温-35度时候把输入电压设置为220VAC,可以正常启动,接着把输入电压减小为105VAC,输出电压可以带载。我的定位测试如下:
1、当前的输入大电容总容值为18UF(C13和C15之和)。当把总容值改为45UF,上述低温条件下可以正常启动。(但是我的PCB面积限制,只能使用18UF左右的电容)
2、在常温下,输入大电容总容值10UF的时候,输入电源105VAC,可以带载5W,但是总容值8UF就不能带载5W。
3、根据文档《Analysis of Start-Up Performance for UCC28700》,怀疑UCC28700的VDD电压太低。于是把VDD的电容C18由1UF改为10UF,常温下VDD电压达到30V,但是低温下还是不能正常启动。同时,把初级电流采用电阻R18由1欧姆改为0.66欧姆,低温下还是不能正常启动。接着,给R18并联1NF或者10NF的电容,低温还是不能正常启动。
4、以前调试过程遇到过常温不能启动的问题,是因为给R19并联了100NF的电容,所以把这个电容拿掉了,常温正常启动。
变压器参数是:初级感量700UH,初级、两个次级、辅助的匝数依次是107、25、25、19,匝比和感量也是参照了PMP9018_REVB设计。
麻烦帮忙分析一下,这个问题消耗了很多时间了,我也尝试了很多办法都没有解决,现在进度很紧张。拜托各位了!
附件中,power_105vac_260vac.pdf是我的原理图。

power_105vac_260vac.rar